Mean Well’s XLG-240 240W Constant Power Mode LED Driver Featured in Latest FLS All in 1+ NPI

Summary: The XLG-240 240W constant power mode LED driver from Mean Well is featured in this month’s FLS All in 1+ NPI Newsletter from Future Electronics.

Montreal, Canada – September 24, 2019 – Future Electronics, a global leading distributor of electronic components, is featuring the XLG-240 240W constant power mode LED driver from Mean Well in this month’s FLS All in 1+ NPI Newsletter.

The XLG-240 series is a 240W LED AC/DC driver featuring constant power mode. XLG-240 operates from 100~305VAC and offers models with different rated current ranging from 700mA to 6.66A. Thanks to its high efficiency of up to 93% and its fanless design, the entire series is able to operate from -40 degree C ~ +90 degree C case temperature under free air convection. The metal housing design and IP67 ingress protection level allows this series to serve both indoor and outdoor applications.

Stay up to date with the latest technology in sensing, IoT and connectivity solutions, subscribe to our newsletter, To see the entire portfolio of Mean Well products available through Future Electronics, visit: www.FutureElectronics.com.

About Future Electronics
Future Electronics is a global leader in electronics distribution, recognized for providing customers with global supply chain solutions, custom-tailored engineering services and a comprehensive suite of passives and semiconductor products. Founded by Robert Miller in 1968, Future Electronics has over 5,500 employees and operates in 169 offices in 44 countries around the world. Future Electronics is globally integrated, with a unified IT infrastructure that delivers real-time inventory availability and access to customers. With the highest level of service, the most advanced engineering capabilities, and the largest available-to-sell inventory in the world, Future’s mission is always to Delight the Customer®. For more information, visit: www.FutureElectronics.com.

Media Contact
Martin H. Gordon
Director, Corporate Communications
FUTURE ELECTRONICS
www.FutureElectronics.com

514-694-7710 (ext. 2236)
Fax: 514-630-2671
martin.gordon@FutureElectronics.com