Summary: Future Electronics is featuring Diodes Incorporated’s versatile AP3917 AC-DC buck converters in the latest issue of Future Technology Magazine.
Montreal, Canada – December 27, 2019 – Future Electronics, a global leading distributor of electronic components, is featuring mains-powered buck converters from Diodes in the latest issue of Future Technology Magazine (FTM).
Diodes Incorporated’s AP3917 family of non-isolated AC-DC switching buck converters are ideal for low-power applications powered by a mains electricity outlet. The AP3917 family consists of the AP3917B, rated for a 170mA nominal load, AP3917C for a 270mA load and the AP3917D, which has a 370mA rating.
The small AP3917 parts offer direct, non-isolated AC-DC conversion at high efficiency, while drawing a low standby current. These attributes are in increasing demand due to the proliferation of small, mains-powered appliances operating as either stand-alone devices or as IoT endpoints.
The AP3917 family features 200µA operating current and a 2W power rating, frequency modulation to suppress EMI, and over-temperature, overload and short-circuit protection. They are perfect for use in home appliances, office equipment, and industrial and IoT devices.
Future Technology Magazine is the flagship publication of Future Electronics, and is geared toward engineers and buyers looking to keep up with the latest developments in the industry. FTM comes out eight times per year, and each issue is packed with new product information, application notes, and detailed technical views from Future’s Advanced Engineers and other industry experts. The magazine is available in both digital and print editions.
Click www.FutureElectronics.com/subscribe to subscribe to Future Technology Magazine. To see the entire portfolio of Diodes products available through Future Electronics, visit www.FutureElectronics.com.
About Future Electronics
Future Electronics is a global leader in electronics distribution, recognized for providing customers with global supply chain solutions, custom-tailored engineering services and a comprehensive suite of passives and semiconductor products. Founded by Robert Miller in 1968, Future Electronics has over 5,500 employees and operates in 169 offices in 44 countries around the world. Future Electronics is globally integrated, with a unified IT infrastructure that delivers real-time inventory availability and access to customers. With the highest level of service, the most advanced engineering capabilities, and the largest available-to-sell inventory in the world, Future’s mission is always to Delight the Customer®. For more information, visit www.FutureElectronics.com.
Media Contact
Martin H. Gordon
Director, Corporate Communications
FUTURE ELECTRONICS
www.FutureElectronics.com
514-694-7710 (ext. 2236)
Fax: 514-630-2671
martin.gordon@FutureElectronics.com