CIPOS Mini IPMs and OPTIGA Trust M Security from Infineon Featured in FTM by Future Electronics

Summary: Future Electronics is featuring Infineon’s CIPOS Mini Intelligent Power Modules and the OPTIGA Trust M security solution in the latest issue of Future Technology Magazine.

Montreal, Canada – January 02, 2020 – Future Electronics, a global leading distributor of electronic components, is featuring intelligent power modules and IoT security solutions from Infineon in the latest issue of Future Technology Magazine (FTM).

Infineon’s energy-efficient CIPOS Mini Intelligent Power Modules (IPMs) integrate the power and control components of an inverter, motor or Power Factor Correction (PFC) power stage in a single package, enabling designers to achieve higher reliability and to optimize PCB size and system cost.

The high level of integration in a CIPOS Mini IPM simplifies the design of power systems and markedly shortens time to market. These IPMs may be used to control AC motors in variable-speed drives consuming up to 3kW.

Infineon’s new OPTIGA Trust M solution helps manufacturers of IoT devices connected to cloud-computing services to enhance the security of their products while also improving system performance.

The OPTIGA Trust M SLS32AIA series, a single-chip security controller solution, stores unique device credentials, and enables devices to connect to the cloud up to ten times faster than software-only alternatives.

When embedded in an IoT end-point device, an SLS32AIA chip can enable security functions including mutual authentication, secure communication, data store protection, lifecycle management, power management, secure updates and platform integrity protection.

Infineon’s Shield2Go board for the OPTIGA Trust M security chip supports fast evaluation and development of IoT end-point devices which require secure cloud connections. It features one OPTIGA Trust M security chip on an easy-to-handle PCB.

Design engineers can build systems by combining multiple Shield2Go boards with the Infineon My IoT adapter board. The adapter board is compatible with the Arduino form factor, and enables fast development in a familiar project environment.

Future Technology Magazine is the flagship publication of Future Electronics, and is geared toward engineers and buyers looking to keep up with the latest developments in the industry. FTM comes out eight times per year, and each issue is packed with new product information, application notes, and detailed technical views from Future’s Advanced Engineers and other industry experts. The magazine is available in both digital and print editions.

Click www.FutureElectronics.com/subscribe to subscribe to Future Technology Magazine. To see the entire portfolio of Infineon products available through Future Electronics, visit www.FutureElectronics.com.

About Future Electronics
Future Electronics is a global leader in electronics distribution, recognized for providing customers with global supply chain solutions, custom-tailored engineering services and a comprehensive suite of passives and semiconductor products. Founded by Robert Miller in 1968, Future Electronics has over 5,500 employees and operates in 169 offices in 44 countries around the world. Future Electronics is globally integrated, with a unified IT infrastructure that delivers real-time inventory availability and access to customers. With the highest level of service, the most advanced engineering capabilities, and the largest available-to-sell inventory in the world, Future’s mission is always to Delight the Customer®. For more information, visit www.FutureElectronics.com.

Media Contact
Martin H. Gordon
Director, Corporate Communications
FUTURE ELECTRONICS
www.FutureElectronics.com

514-694-7710 (ext. 2236)
Fax: 514-630-2671
martin.gordon@FutureElectronics.com