New NCP109x ICs for PoE from ON Semi Featured in FTM by Future Electronics

Summary: Future Electronics is featuring ON Semiconductor’s NCP1095 and NCP1096 interface controllers for high-power PoE in the latest issue of Future Technology Magazine.

Montreal, Canada – January 06, 2019 – Future Electronics, a global leading distributor of electronic components, is featuring the new ICs for power over Ethernet from ON Semiconductor in the latest issue of Future Technology Magazine (FTM).

The NCP1095 and NCP1096 interface controllers from ON Semiconductor provide the high-power PoE capability specified in the IEEE 802.3bt standard. These ICs incorporate all the features needed to implement a PoE interface at the PD, including detection, auto-classification and current limiting.

The controllers are complemented by the NCP1566 DC-DC controller, the FDMC8622 single MOSFET, and the FDMQ8203 and FDMQ8205A GreenBridge Quad MOSFETs, which provide a more efficient alternative to a diode bridge in PoE applications.

Together, these devices enable the designers to create highly efficient PoE interfaces with up to the standard limit of 90W of power, or up to a proprietary 100W solution if more power is needed in applications such as telecoms equipment or digital signage.

Future Technology Magazine is the flagship publication of Future Electronics, and is geared toward engineers and buyers looking to keep up with the latest developments in the industry. FTM comes out eight times per year, and each issue is packed with new product information, application notes, and detailed technical views from Future’s Advanced Engineers and other industry experts. The magazine is available in both digital and print editions.

Click www.FutureElectronics.com/subscribe to subscribe to Future Technology Magazine. To see the entire portfolio of ON Semiconductor products available through Future Electronics, visit www.FutureElectronics.com.

About Future Electronics
Future Electronics is a global leader in electronics distribution, recognized for providing customers with global supply chain solutions, custom-tailored engineering services and a comprehensive suite of passives and semiconductor products. Founded by Robert Miller in 1968, Future Electronics has over 5,500 employees and operates in 169 offices in 44 countries around the world. Future Electronics is globally integrated, with a unified IT infrastructure that delivers real-time inventory availability and access to customers. With the highest level of service, the most advanced engineering capabilities, and the largest available-to-sell inventory in the world, Future’s mission is always to Delight the Customer®. For more information, visit www.FutureElectronics.com.

Media Contact
Martin H. Gordon
Director, Corporate Communications
FUTURE ELECTRONICS
www.FutureElectronics.com

514-694-7710 (ext. 2236)
Fax: 514-630-2671
martin.gordon@FutureElectronics.com