Summary: Future Electronics is featuring Triad Magnetics’ CMF series of Dual Mode Chokes in the latest issue of Future Technology Magazine.
Montreal, Canada – January 11, 2020– Future Electronics, a global leading distributor of electronic components, is featuring Dual Mode Chokes from Triad Magnetics in the latest issue of Future Technology Magazine (FTM).
The CMF Series of Dual Mode Chokes from Triad Magnetics combine both DM and CM noise-suppressing approaches into a dual-function, open-frame design that provides the features of both chokes in a single, smaller, more cost-effective package.
The CMF series represents far more than a co-packaging of two devices into a single component. Instead, their design enhances electrical performance while yielding savings in size and cost.
There are 21 CMF models with current ratings from 0.45 to 2.3A, inductances from 10 to 100mH, and stray inductances from 200 to 2100mH. DC resistances are 188 to 2930mΩ, depending on model. They are available in horizontal and vertical packages to fit tight clearance situations.
Despite their small size, the creepage and clearance parameter is greater than 3mm and they are rated for 300VAC operation. They are an excellent solution for most designs.
Future Technology Magazine is the flagship publication of Future Electronics, and is geared toward engineers and buyers looking to keep up with the latest developments in the industry. FTM comes out eight times per year, and each issue is packed with new product information, application notes, and detailed technical views from Future’s Advanced Engineers and other industry experts. The magazine is available in both digital and print editions.
Click www.FutureElectronics.com/subscribe to subscribe to Future Technology Magazine. To see the entire portfolio of Triad Magnetics products available through Future Electronics, visit www.FutureElectronics.com.
About Future Electronics
Future Electronics is a global leader in electronics distribution, recognized for providing customers with global supply chain solutions, custom-tailored engineering services and a comprehensive suite of passives and semiconductor products. Founded by Robert Miller in 1968, Future Electronics has over 5,500 employees and operates in 169 offices in 44 countries around the world. Future Electronics is globally integrated, with a unified IT infrastructure that delivers real-time inventory availability and access to customers. With the highest level of service, the most advanced engineering capabilities, and the largest available-to-sell inventory in the world, Future’s mission is always to Delight the Customer®. For more information, visit www.FutureElectronics.com.
Media Contact
Martin H. Gordon
Director, Corporate Communications
FUTURE ELECTRONICS
www.FutureElectronics.com
514-694-7710 (ext. 2236)
Fax: 514-630-2671
martin.gordon@FutureElectronics.com