CMF Dual Mode Chokes from Triad Magnetics Featured in FTM by Future Electronics

Summary: Future Electronics is featuring Triad Magnetics’ CMF series of Dual Mode Chokes in the latest issue of Future Technology Magazine.

Montreal, Canada – January 11, 2020– Future Electronics, a global leading distributor of electronic components, is featuring Dual Mode Chokes from Triad Magnetics in the latest issue of Future Technology Magazine (FTM).

The CMF Series of Dual Mode Chokes from Triad Magnetics combine both DM and CM noise-suppressing approaches into a dual-function, open-frame design that provides the features of both chokes in a single, smaller, more cost-effective package.

The CMF series represents far more than a co-packaging of two devices into a single component. Instead, their design enhances electrical performance while yielding savings in size and cost.

There are 21 CMF models with current ratings from 0.45 to 2.3A, inductances from 10 to 100mH, and stray inductances from 200 to 2100mH. DC resistances are 188 to 2930mΩ, depending on model. They are available in horizontal and vertical packages to fit tight clearance situations.

Despite their small size, the creepage and clearance parameter is greater than 3mm and they are rated for 300VAC operation. They are an excellent solution for most designs.

Future Technology Magazine is the flagship publication of Future Electronics, and is geared toward engineers and buyers looking to keep up with the latest developments in the industry. FTM comes out eight times per year, and each issue is packed with new product information, application notes, and detailed technical views from Future’s Advanced Engineers and other industry experts. The magazine is available in both digital and print editions.

Click www.FutureElectronics.com/subscribe to subscribe to Future Technology Magazine. To see the entire portfolio of Triad Magnetics products available through Future Electronics, visit www.FutureElectronics.com.

About Future Electronics
Future Electronics is a global leader in electronics distribution, recognized for providing customers with global supply chain solutions, custom-tailored engineering services and a comprehensive suite of passives and semiconductor products. Founded by Robert Miller in 1968, Future Electronics has over 5,500 employees and operates in 169 offices in 44 countries around the world. Future Electronics is globally integrated, with a unified IT infrastructure that delivers real-time inventory availability and access to customers. With the highest level of service, the most advanced engineering capabilities, and the largest available-to-sell inventory in the world, Future’s mission is always to Delight the Customer®. For more information, visit www.FutureElectronics.com.

Media Contact
Martin H. Gordon
Director, Corporate Communications
FUTURE ELECTRONICS
www.FutureElectronics.com

514-694-7710 (ext. 2236)
Fax: 514-630-2671
martin.gordon@FutureElectronics.com

PAN4620 Radio Module and EKMB/EKMC PIR Sensors from Panasonic Featured in FTM by Future Electronics

Summary: Future Electronics is featuring Panasonic’s PAN4620 dual-mode radio module and EKMB/EKMC low-profile PIR motion sensors in the latest issue of Future Technology Magazine.

Montreal, Canada – January 07, 2020 – Future Electronics, a global leading distributor of electronic components, is featuring new motion sensors and radio modules from Panasonic in the latest issue of Future Technology Magazine (FTM).

Panasonic’s EKMB and EKMC series now include new low-profile Passive Infrared (PIR) motion sensors. Featuring a new lens design, the low-profile PIR sensors are 10.9mm high, while regular EKMC and EKMB products are 14.4mm high, and they have a detection range of 5m.

EKMB and EKMC PIR motion sensors are an ideal solution for lighting controls, thermostats, HVAC units, smart home equipment, IoT devices, IP cameras, surveillance systems, and digital signage.

Panasonic’s PAN4620 is a dual-mode radio module which enables simultaneous and independent connections over Bluetooth Low Energy and Thread or other 2.4GHz IEEE 802.15.4 wireless networks.

The module incorporates all the required hardware elements, including a chip antenna, and the protocol software, providing a simple and quick way for OEMs to implement wireless connectivity in devices for applications such as smart homes and building automation.

Panasonic also provides an evaluation board for its combination 802.15.4 and Bluetooth radio module. The compact PAN4620 daughterboard provides access to all the module’s pins. It also features an on-board LED, three user buttons and a Micro-USB connector.

Future Technology Magazine is the flagship publication of Future Electronics, and is geared toward engineers and buyers looking to keep up with the latest developments in the industry. FTM comes out eight times per year, and each issue is packed with new product information, application notes, and detailed technical views from Future’s Advanced Engineers and other industry experts. The magazine is available in both digital and print editions.

Click www.FutureElectronics.com/subscribe to subscribe to Future Technology Magazine. To see the entire portfolio of Panasonic products available through Future Electronics, visit www.FutureElectronics.com.

About Future Electronics
Future Electronics is a global leader in electronics distribution, recognized for providing customers with global supply chain solutions, custom-tailored engineering services and a comprehensive suite of passives and semiconductor products. Founded by Robert Miller in 1968, Future Electronics has over 5,500 employees and operates in 169 offices in 44 countries around the world. Future Electronics is globally integrated, with a unified IT infrastructure that delivers real-time inventory availability and access to customers. With the highest level of service, the most advanced engineering capabilities, and the largest available-to-sell inventory in the world, Future’s mission is always to Delight the Customer®. For more information, visit www.FutureElectronics.com.

Media Contact
Martin H. Gordon
Director, Corporate Communications
FUTURE ELECTRONICS
www.FutureElectronics.com

514-694-7710 (ext. 2236)
Fax: 514-630-2671
martin.gordon@FutureElectronics.com

Mean Well’s SLD-80 Dual Mode Linear LED Driver Featured in Latest FLS All in 1+ NPI Newsletter

Summary: The SLD-80 dual mode linear LED driver from Mean Well is featured in this month’s FLS All in 1+ NPI Newsletter from Future Electronics.

Montreal, Canada – October 08, 2019 – Future Electronics, a global leading distributor of electronic components, is featuring the SLD-80 dual mode linear LED driver from Mean Well in this month’s FLS All in 1+ NPI Newsletter.

The SLD-80 series is an 80W AC/DC LED driver featuring dual modes, constant voltage and constant current output. SLD-80 operates from 110~305 VAC and feature models with different rated voltage from 12V to 56V. The SLD-80 is designed with a low profile and a linear housing, making it ideal for signage and linear luminaire applications.

Click here to subscribe to the FLS All in 1+ NPI Newsletter, featuring the latest in lighting technology. To see the entire portfolio of Mean Well products available through Future Electronics, visit: www.FutureElectronics.com.

About Future Electronics
Future Electronics is a global leader in electronics distribution, recognized for providing customers with global supply chain solutions, custom-tailored engineering services and a comprehensive suite of passives and semiconductor products. Founded by Robert Miller in 1968, Future Electronics has over 5,500 employees and operates in 169 offices in 44 countries around the world. Future Electronics is globally integrated, with a unified IT infrastructure that delivers real-time inventory availability and access to customers. With the highest level of service, the most advanced engineering capabilities, and the largest available-to-sell inventory in the world, Future’s mission is always to Delight the Customer®. For more information, visit: www.FutureElectronics.com.

Media Contact
Martin H. Gordon
Director, Corporate Communications
FUTURE ELECTRONICS
www.FutureElectronics.com

514-694-7710 (ext. 2236)
Fax: 514-630-2671
martin.gordon@FutureElectronics.com

NCP171 50 nA Iq Dual Mode LDO Regulator from ON Semi Featured in THE EDGE by Future Electronics

Summary: Future Electronics is featuring ON Semiconductor’s NCP171 50 nA Iq dual mode LDO regulator in this month’s edition of THE EDGE.

Montreal, Canada – August 14, 2019 – Future Electronics, a global leading distributor of electronic components, is featuring the NCP171 50 nA Iq dual mode LDO regulator from ON Semiconductor in the latest edition of THE EDGE.

The NCP171 is a dual mode LDO offering up to 80 mA in Active Mode and as low as 50 nA of Iq in Low Power Mode. The Dual Mode function is selectable with the ECO pin allowing for dynamic switching between Active and Low Power modes, ideal for long-life battery-powered wireless applications. The output voltage in Low Power mode can be lowered by a pre-programmed value ranging from 50 mV, 100 mV, 150 mV or 200 mV, further lowering the application consumption in sleep mode.

THE EDGE is the latest e-newsletter from Future Electronics, and is geared toward engineers and buyers looking for new or leading-edge products. THE EDGE comes out twice per month, and each edition features product information, datasheets and videos showcasing the most advanced new technology in a specific area, such as connectivity, lighting, or automotive.

Click here to view the most recent edition of THE EDGE, featuring the latest in power management solutions. To see the entire portfolio of ON Semiconductor products available through Future Electronics, visit www.FutureElectronics.com.

About Future Electronics
Future Electronics is a global leader in electronics distribution, recognized for providing customers with global supply chain solutions, custom-tailored engineering services and a comprehensive suite of passives and semiconductor products. Founded by Robert Miller in 1968, Future Electronics has over 5,500 employees and operates in 169 offices in 44 countries around the world. Future Electronics is globally integrated, with a unified IT infrastructure that delivers real-time inventory availability and access to customers. With the highest level of service, the most advanced engineering capabilities, and the largest available-to-sell inventory in the world, Future’s mission is always to Delight the Customer®. For more information, visit www.FutureElectronics.com.

Media Contact
Martin H. Gordon
Director, Corporate Communications
FUTURE ELECTRONICS
www.FutureElectronics.com

514-694-7710 (ext. 2236)
Fax: 514-630-2671
martin.gordon@FutureElectronics.com

THE EDGE by Future Electronics Features Cypress’ new CYW20719 Dual-Mode Bluetooth 5.0 Wireless MCU

Montreal, Canada – July 30, 2018 – Future Electronics, a global leading distributor of electronic components, is featuring the new CYW20719 dual-mode Bluetooth 5.0 wireless MCU from Cypress in the latest edition of THE EDGE.

Cypress’ new CYW20719 dual-mode Bluetooth 5.0 wireless MCU enables power-efficient and highly-integrated IoT designs, and is supported in WICED® Studio. An evaluation kit is available with on-board sensors and example projects to easily prototype IoT designs, and a certified CYW20719 based module is available to speed up the design cycle.

THE EDGE is the latest e-newsletter from Future Electronics, and is geared toward engineers and buyers looking for new or leading-edge products. THE EDGE comes out twice per month, and each edition features product information, datasheets and videos showcasing the most advanced new technology in a specific area, such as sensing, lighting, or automotive.

Click here to view the most recent edition of THE EDGE, featuring the latest in intelligent sensing solutions. To see the entire portfolio of Cypress products available through Future Electronics, visit: www.FutureElectronics.com

About Future Electronics

Future Electronics is a global leader in electronics distribution, ranking 3rd in component sales worldwide, with an impressive reputation for developing efficient, comprehensive global supply chain solutions, as well as differentiated engineering services encompassing technical support, technology training and custom board design. Founded in 1968 by Robert Miller, President, Future Electronics has established itself as one of the most innovative organizations in the industry today, with 5,500 employees in 169 offices in 44 countries around the world. Future Electronics is globally integrated, with one worldwide IT infrastructure providing real-time inventory availability and access, while enabling full integration of its operations, sales and marketing worldwide. Offering the highest level of service, the most advanced engineering capabilities and technical solutions through all stages of the design-production cycle, and the largest available-to-sell inventory in the world, Future’s mission is always to Delight the Customer®. For more information, visit www.FutureElectronics.com.

Future Electronics Introduces Industry’s First Dual-Mode Battery Charging IC from ROHM

Montreal, Canada – April 5, 2018 – Future Electronics, a global leading distributor of electronic components, is very pleased to announce the immediate availability of ROHM’s BD99954GW/MUV dual-mode battery charging IC, a true first in the industry.

A growing number of portable devices, including notebook PCs, are adopting the USB Type-C PD standard that can charge up to 100W, providing a common charging platform. At the same time, wireless charging is gaining traction, increasing the demand to support both charging methods.

But delivering the wide power supply range required by USBPD requires an added boost function, and enabling two simultaneous charging methods to operate at the same time requires charge ICs and an MCU to control charge switching, presenting a significant barrier to introduction.

By combining its USBPD IC with proprietary semiconductor technologies, ROHM has met these needs, delivering dual-input charging ICs that support multiple power input sources.

The BD99954 delivers an output voltage between 3.07 and 19.2V to support 1-to-4-cell batteries through a buck-boost DCDC controller. On the input side, support for voltages between 3.8V and 25V is provided, covering the voltage range (5V to 20V) defined by USB PD. The industry’s first dual-input charging system can autonomously select from two inputs without an MCU and provide the necessary voltage and current to charge the battery.

The IC is also compatible with both USBPD and USB BC 1.2, facilitating configuration of dual-mode systems capable of simultaneous charging via USBPD, wirelessly, or from legacy USB adapters.

ROHM’s BD99954GW/MUV dual-mode battery charging IC is available now from Future Electronics. For more information and to watch a video about this product, click here. To see the entire portfolio of ROHM products available through Future Electronics, visit: www.FutureElectronics.com

About Future Electronics

Future Electronics is a global leader in electronics distribution, ranking 3rd in component sales worldwide, with an impressive reputation for developing efficient, comprehensive global supply chain solutions, as well as differentiated engineering services encompassing technical support, technology training and custom board design. Founded in 1968 by Robert Miller, President, Future Electronics has established itself as one of the most innovative organizations in the industry today, with 5,500 employees in 169 offices in 44 countries around the world. Future Electronics is globally integrated, with one worldwide IT infrastructure providing real-time inventory availability and access, while enabling full integration of its operations, sales and marketing worldwide. Offering the highest level of service, the most advanced engineering capabilities and technical solutions through all stages of the design-production cycle, and the largest available-to-sell inventory in the world, Future’s mission is always to Delight the Customer®. For more information, visit www.FutureElectronics.com.

 

Media Contact
Martin H. Gordon
Director, Corporate Communications
FUTURE ELECTRONICS
www.FutureElectronics.com

514-694-7710 (ext. 2236)
Fax: 514-630-2671
martin.gordon@FutureElectronics.com