Montreal, Canada – June 28, 2018 – Future Electronics, a global leading distributor of electronic components, now carries Panasonic’s new fully embedded standalone Wi-Fi module and combo Wi-Fi and Bluetooth module.
The PAN9420 is a fully embedded standalone Wi-FI module device perfect for design engineers with limited Wi-Fi experience or for applications that must be implemented with minimal time and effort.
The PAN9026 is a Wi-Fi radio module integrating Wi-Fi and Bluetooth wireless connectivity that allows applications such as Smart Energy and home gateways to manage multiple devices and appliances. The combination of Wi-Fi and Bluetooth provides the highest flexibility for connectivity.
Both modules are excellent solutions for highly integrated and cost-effective applications such as white goods, vending machines and home appliances.
The PAN9420 is a 2.4 GHz 802.11 b/g/n Embedded Wi-Fi Module with integrated stack and API that minimizes firmware development and includes a full security suite. The module includes a fully shielded case, integrated crystal oscillators and a chip antenna. The PAN9420 Series combines a high-performance CPU, high-sensitivity wireless radio, baseband processor, medium access controller, encryption unit, boot ROM with patching capability, internal SRAM and in-system programmable flash memory.
The PAN9026 is a dual band 2.4/5 GHz 802.11 a/b/g/n module integrating Wi-Fi and Bluetooth. The simultaneous and independent operation of the two standards enables high data rates (802.11n) and low-power operation (Bluetooth Low Energy). Integrated power management, a fast dual-core CPU, 802.11i security standard support, and high-speed data interfaces deliver the performance for the speed, reliability, and quality requirements of next generation products.
For more information and to watch a video about these products, click here. To see the full portfolio of Panasonic products available through Future Electronics, visit: www.FutureElectronics.com.
About Future Electronics
Future Electronics is a global leader in electronics distribution, ranking 3rd in component sales worldwide, with an impressive reputation for developing efficient, comprehensive global supply chain solutions, as well as differentiated engineering services encompassing technical support, technology training and custom board design. Founded in 1968 by Robert Miller, President, Future Electronics has established itself as one of the most innovative organizations in the industry today, with 5,500 employees in 169 offices in 44 countries around the world. Future Electronics is globally integrated, with one worldwide IT infrastructure providing real-time inventory availability and access, while enabling full integration of its operations, sales and marketing worldwide. Offering the highest level of service, the most advanced engineering capabilities and technical solutions through all stages of the design-production cycle, and the largest available-to-sell inventory in the world, Future’s mission is always to Delight the Customer®. For more information, visit www.FutureElectronics.com.
Media Contact
Martin H. Gordon
Director, Corporate Communications
FUTURE ELECTRONICS
www.FutureElectronics.com
514-694-7710 (ext. 2236)
Fax: 514-630-2671
martin.gordon@FutureElectronics.com