Renesas RX13T 32 Bit Microcontrollers Introduced by Future Electronics

For Immediate Release:

Summary:

Future Electronics is featuring the Renesas RX13T series of 32 bit microcontrollers (MCU).

Press Release:

Montreal, Canada – April 14, 2020 – Future Electronics, a global leading distributor of electronic components, is introducing Renesas’ RX13T family of 32 bit microcontrollers.

The RX13T group of microcontrollers is used for efficient inverter control of compact motors such as fans or pumps in consumer and industrial applications.

Renesas 32 bit MCUs are equipped with the proven RX Family RXv1 core, which operates at 32MHz. They feature a floating point unit (FPU), an inverter control timer and a 12-bit A/D converter, allowing high-efficiency inverter control of brushless DC motors with one device.

Renesas RX13T MCUs are highly compatible with existing RX devices, making it easy to convert hardware and software from previous designs. The lineup includes small 32-pin and 48-pin packages with built-in features such as programmable gain amplifier (PGA), comparator, data flash, and high-speed on-chip oscillator (HOCO). These on-chip features can help reduce board area and the BOM components in the design.

Visit http://www.FutureElectronics.com/subscribe to receive the latest Future Electronics newsletters to continuously stay up to date with the latest innovations of the technology world. To see the entire portfolio of components available through Future Electronics, visit www.FutureElectronics.com.

About Future Electronics
Future Electronics is a global leader in electronics distribution, recognized for providing customers with global supply chain solutions, custom-tailored engineering services and a comprehensive suite of passives and semiconductor products. Founded by Robert Miller in 1968, Future Electronics has over 5,500 employees and operates in 170 offices in 44 countries around the world. Future Electronics is globally integrated, with a unified IT infrastructure that delivers real-time inventory availability and access to customers. With the highest level of service, the most advanced engineering capabilities, and the largest available-to-sell inventory in the world, Future’s mission is always to Delight the Customer®. For more information, visit www.FutureElectronics.com.

Media Contact
Martin H. Gordon
Director, Corporate Communications
FUTURE ELECTRONICS
www.FutureElectronics.com

514-694-7710 (ext. 2236)
Fax: 514-630-2671
martin.gordon@FutureElectronics.com