Future Electronics Immediate Shipping Availability of MEAN WELL’s New LRS Series

MONTREAL – December 14, 2017 – Future Electronics, a global leading distributor of electronic components, is offering immediate shipping availability of MEAN WELL’s LRS Series new generation industrial standard power supplies.

MEAN WELL recently unveiled its new generation 35~350W “without PFC” LRS enclosed type family. The LRS family exploits a streamlined circuitry design that lowers the electrical component count, and high-degree automation is introduced which significantly raises the cost competitiveness and production yield.

Compared to the former generation, the RS series, it has a higher efficiency and is better miniaturized. It also has the supreme attributes such as low no load consumption (< 0.2~0.75W), 1U low profile (30mm) and the capability of operating at altitudes up to 5000m. In addition, this family complies with various safety regulation standards, including IEC/EN/UL60950-1, IEC/EN61558-1, IEC/EN61558-2-16, IEC/EN60335-1, GB4943, etc.

It not only satisfies every kind of industrial related applications but can also be utilized for household appliances, and it thus accounts for a broader coverage for diverse industries.

The LRS-35 Series is a 35W single-output enclosed type power supply with 30mm of low profile design. Adopting the full range 85 – 264 VAC input, the entire series provides an output voltage of 5V, 12V, 15V, 24V, 36V and 48V. The LRS-50 Series is a 50W single-output enclosed type power supply with 30mm of low profile design. Adopting the full range 85 – 264 VAC input, the entire series provides an output voltage of 3.3V, 5V, 12V, 15V, 24V, 36V and 48V. The LRS-75 Series is a 75W single-output enclosed type power supply with 30mm of low profile design. Adopting the full range 85 – 264 VAC input, the entire series provides an output voltage of 5V, 12V, 15V, 24V, 36V and 48V.

The LRS-100 Series is a 100W single-output enclosed type power supply with 30mm of low profile design. Adopting the full range 85 – 264 VAC input, the entire series provides an output voltage of 3.3V, 5V, 12V, 15V, 24V, 36V and 48V. The LRS-150 Series and LRS-150R Series are 150W single-output enclosed type power supply with 30mm of low profile design. The entire series provides an output voltage of 5V, 12V, 15V, 24V, 36V and 48V. The LRS-200 Series is a 200W single-output enclosed type power supply with 30mm of low profile design. Adopting the full range 85 – 264 VAC input, the entire series provides an output voltage of 3.3V, 4.2V, 5V, 12V, 15V, 24V, 36V and 48V. The LRS-350 Series is a 350W single-output enclosed type power supply with 30mm of low profile design. Adopting the full range 85 – 264 VAC input, the entire series provides an output voltage of 3.3V, 4.2V, 5V, 12V, 15V, 24V, 36V and 48V.

For more information about the LRS Series and other MEAN WELL products available through Future Electronics, as well as access to the world’s largest available-to-sell inventory, visit: www.FutureElectronics.com

About Future Electronics
Future Electronics is a global leader in electronics distribution, ranking 3rd in component sales worldwide, with an impressive reputation for developing efficient, comprehensive global supply chain solutions, as well as providing differentiated engineering services encompassing technical support, technology training and custom board design. Founded in 1968 by Robert Miller, President, Future Electronics has established itself as one of the most innovative organizations in the industry today, with 5,500 employees in 169 offices in 44 countries around the world. Future Electronics is globally integrated, with one worldwide IT infrastructure providing real-time inventory availability and access, while enabling full integration of its operations, sales and marketing worldwide. Offering the highest level of service, the most advanced engineering capabilities and technical solutions through all stages of the design-production cycle, and the largest available-to-sell inventory in the world, Future’s mission is always to Delight the Customer®.

For more information, visit www.FutureElectronics.com.

Media Contact
Martin H. Gordon
Director, Corporate Communications
FUTURE ELECTRONICS
www.FutureElectronics.com

514-694-7710 (ext. 2236)
Fax: 514-630-2671
martin.gordon@FutureElectronics.com