Summary: Future Electronics is featuring Panasonic’s PAN4620 dual-mode radio module and EKMB/EKMC low-profile PIR motion sensors in the latest issue of Future Technology Magazine.
Montreal, Canada – January 07, 2020 – Future Electronics, a global leading distributor of electronic components, is featuring new motion sensors and radio modules from Panasonic in the latest issue of Future Technology Magazine (FTM).
Panasonic’s EKMB and EKMC series now include new low-profile Passive Infrared (PIR) motion sensors. Featuring a new lens design, the low-profile PIR sensors are 10.9mm high, while regular EKMC and EKMB products are 14.4mm high, and they have a detection range of 5m.
EKMB and EKMC PIR motion sensors are an ideal solution for lighting controls, thermostats, HVAC units, smart home equipment, IoT devices, IP cameras, surveillance systems, and digital signage.
Panasonic’s PAN4620 is a dual-mode radio module which enables simultaneous and independent connections over Bluetooth Low Energy and Thread or other 2.4GHz IEEE 802.15.4 wireless networks.
The module incorporates all the required hardware elements, including a chip antenna, and the protocol software, providing a simple and quick way for OEMs to implement wireless connectivity in devices for applications such as smart homes and building automation.
Panasonic also provides an evaluation board for its combination 802.15.4 and Bluetooth radio module. The compact PAN4620 daughterboard provides access to all the module’s pins. It also features an on-board LED, three user buttons and a Micro-USB connector.
Future Technology Magazine is the flagship publication of Future Electronics, and is geared toward engineers and buyers looking to keep up with the latest developments in the industry. FTM comes out eight times per year, and each issue is packed with new product information, application notes, and detailed technical views from Future’s Advanced Engineers and other industry experts. The magazine is available in both digital and print editions.
Click www.FutureElectronics.com/subscribe to subscribe to Future Technology Magazine. To see the entire portfolio of Panasonic products available through Future Electronics, visit www.FutureElectronics.com.
About Future Electronics
Future Electronics is a global leader in electronics distribution, recognized for providing customers with global supply chain solutions, custom-tailored engineering services and a comprehensive suite of passives and semiconductor products. Founded by Robert Miller in 1968, Future Electronics has over 5,500 employees and operates in 169 offices in 44 countries around the world. Future Electronics is globally integrated, with a unified IT infrastructure that delivers real-time inventory availability and access to customers. With the highest level of service, the most advanced engineering capabilities, and the largest available-to-sell inventory in the world, Future’s mission is always to Delight the Customer®. For more information, visit www.FutureElectronics.com.
Media Contact
Martin H. Gordon
Director, Corporate Communications
FUTURE ELECTRONICS
www.FutureElectronics.com
514-694-7710 (ext. 2236)
Fax: 514-630-2671
martin.gordon@FutureElectronics.com