Future Electronics Offers Low-Power, High-Precision Operational Amplifiers from Microchip

Montreal, Canada – April 19, 2018 – Future Electronics, a global leading distributor of electronic components, is pleased to announce the immediate availability of Microchip’s MCP6031 operational amplifier and Photodiode PICtail™ Plus Demo Board.

Future Electronics customers will benefit from the high accuracy and extended battery life delivered by these operational amplifiers. Microchip’s low-power Complementary Metal–Oxide–Semiconductor (CMOS) technology and implementation of non-volatile memory for in-package trimming enable the MCP6031/2/3/4 amplifiers’ extremely low offset. This minimizes error, especially at higher gains.

Additionally, with an operating voltage range of 1.8V to 5.5V, the amplifiers can run off of two 1.5V battery cells with full battery utilization. Their low power consumption extends battery life, and their rail-to-rail input/output structure enables greater dynamic range and better performance across the entire operating-voltage range.

The MCP6031 Photodiode PICtail™ Plus Demo Board is also available from Future Electronics. It supports the Microchip MCP6031 high precision op amp, and uses a transimpedance amplifier as a sensor conditioning circuit, and a PIN photodiode (PNZ334) as a light detector. It also features test points for connecting lab equipment.

Microchip’s MCP6031 operational amplifier and Photodiode PICtail™ Plus Demo Board are available now from Future Electronics. For more information and to watch a video about this product, click here. To see the entire portfolio of Microchip products available through Future Electronics, visit: www.FutureElectronics.com

About Future Electronics

Future Electronics is a global leader in electronics distribution, ranking 3rd in component sales worldwide, with an impressive reputation for developing efficient, comprehensive global supply chain solutions, as well as differentiated engineering services encompassing technical support, technology training and custom board design. Founded in 1968 by Robert Miller, President, Future Electronics has established itself as one of the most innovative organizations in the industry today, with 5,500 employees in 169 offices in 44 countries around the world. Future Electronics is globally integrated, with one worldwide IT infrastructure providing real-time inventory availability and access, while enabling full integration of its operations, sales and marketing worldwide. Offering the highest level of service, the most advanced engineering capabilities and technical solutions through all stages of the design-production cycle, and the largest available-to-sell inventory in the world, Future’s mission is always to Delight the Customer®. For more information, visit www.FutureElectronics.com.

 

Media Contact
Martin H. Gordon
Director, Corporate Communications
FUTURE ELECTRONICS
www.FutureElectronics.com

514-694-7710 (ext. 2236)
Fax: 514-630-2671
martin.gordon@FutureElectronics.com