MAX22200 Octal Solenoid Driver from Maxim Integrated Featured in THE EDGE by Future Electronics

Summary: Future Electronics is featuring Maxim Integrated’s MAX22200 octal 36V serial-controlled solenoid driver in this month’s Motor Control edition of THE EDGE.

Montreal, Canada – Future Electronics, a global leading distributor of electronic components, is featuring energy efficient drivers from Maxim Integrated in the latest edition of THE EDGE – Motor Control.

The Maxim Integrated MAX22200 is an octal 36V serial-controlled solenoid driver featuring a full set of protections and diagnostic functions for flexibility of use in multiple applications. This includes overcurrent protection (OCP), thermal shutdown (TSD), undervoltage Lockout (UVLO), open-load detection (OL), and detection of plunger movement (DPM). A fault indication pin (active-low FAULT) signals fault events and diagnostic information is stored in the FAULT register.

The MAX22200 is available in a compact 5mm x 5mm, 32-pin TQFN package and operates over the temperature -40°C to +85°C range. Due to the flexibility of use, the serial interface control, the high efficiency, and the small package, the MAX22200 is particularly well-suited for solenoid driver applications such as valve control, relays control, etc. in which low power consumption and a high level of integration are required.

To learn more, visit, https://www.futureelectronics.com/resources/featured-products/maxim-integrated-max22200. To see the entire portfolio of Maxim Integrated products available through Future Electronics, visit www.FutureElectronics.com.

THE EDGE is the latest e-newsletter from Future Electronics, and is geared toward engineers and buyers looking for new or leading-edge products. THE EDGE comes out twice per month, and each edition features product information, datasheets and videos showcasing the most advanced new technology in a specific area, such as sensing, lighting, or automotive.

Visit www.FutureElectronics.com/subscribe to receive the latest issues of THE EDGE newsletter, and stay up to date with the newest technologies. 

About Future Electronics
Future Electronics is a global leader in electronics distribution, recognized for providing customers with global supply chain solutions, custom-tailored engineering services and a very extensive variety of electronic components. Founded by Robert G. Miller in 1968, Future Electronics believes its 5500 employees are its greatest asset, with 170 offices in 44 countries. Future Electronics is globally integrated, with a unified IT infrastructure that delivers real-time inventory availability and access to customers. With the highest level of service, the most advanced engineering capabilities, and the largest available-to-sell inventory in the world, Future’s mission is always to Delight the Customer®. For more information, visit www.FutureElectronics.com.

Media contact:
Claudio Caporicci
Global Director Marketing Communications & Advertising
FUTURE ELECTRONICS
www.FutureElectronics.com
+1 514-694-7710
Claudio.Caporicci@FutureElectronics.com