EZP-V Capacitors from Panasonic Featured in THE EDGE by Future Electronics

Summary: Future Electronics is featuring Panasonic’s EZP-V Series of Metallized Polypropylene Plastic Film Capacitors in this month’s Transportation edition of THE EDGE.

Montreal, Canada – Future Electronics, a global leading distributor of electronic components, is featuring advanced capacitors from Panasonic in the latest edition of THE EDGE – Transportation.

Panasonic’s EZP-V Series Metallized Polypropylene Plastic Film Capacitors feature a built-in fuse function combined with a small case size, which makes them ideal for applications requiring DC linkage. Built-in fuse functionality ensures that EZP-V Series parts open in the event of an unlikely failure, rather than creating a short circuit situation.

EZP-V Series capacitors deliver the stability and reliability needed for major applications such as solar inverters and wind power generation. Key highlights include a wide operating temperature range of -40°C up to +105°C, a rated voltage range of 600VDC to 1100VDC and a nominal capacitance range of 3µF up to 110µF.

To learn more, visit, www.futureelectronics.com/resources/featured-products/panasonic-ezp-v-metallized-polypropylene-plastic-film-capacitors. To see the entire portfolio of Panasonic products available through Future Electronics, visit www.FutureElectronics.com.

THE EDGE is the latest e-newsletter from Future Electronics, and is geared toward engineers and buyers looking for new or leading-edge products. THE EDGE comes out twice per month, and each edition features product information, datasheets and videos showcasing the most advanced new technology in a specific area, such as sensing, lighting, or automotive.

Visit www.FutureElectronics.com/subscribe to receive the latest issues of THE EDGE newsletter, and stay up to date with the newest technologies. 

About Future Electronics
Future Electronics is a global leader in electronics distribution, recognized for providing customers with global supply chain solutions, custom-tailored engineering services and a very extensive variety of electronic components. Founded by Robert G. Miller in 1968, Future Electronics believes its 5500 employees are its greatest asset, with 170 offices in 44 countries. Future Electronics is globally integrated, with a unified IT infrastructure that delivers real-time inventory availability and access to customers. With the highest level of service, the most advanced engineering capabilities, and the largest available-to-sell inventory in the world, Future’s mission is always to Delight the Customer®. For more information, visit www.FutureElectronics.com.

Media contact:
Claudio Caporicci
Global Director Marketing Communications & Advertising
FUTURE ELECTRONICS
www.FutureElectronics.com
+1 514-694-7710
Claudio.Caporicci@FutureElectronics.com