For Immediate Release:
Summary:
Future Electronics has introduced the Maxim Integrated MAX3301 family of Control Area Network transceivers.
Press Release:
Montreal, Canada – April 20, 2020 – Future Electronics, a global leading distributor of electronic components, is introducing the Maxim Integrated MAX3301 group of CAN transceivers.
These industry-first Control Area Network transceivers are part of a +5V family that include integrated protection for industrial applications. The MAX33011E–MAX33012E, and MAX33014E–MAX33015E devices have extended ±65V fault protection on the CAN bus for equipment where overvoltage protection is required. The CAN family also incorporates high ±45kV ESD HBM protection and an input common mode range (CMR) of ±25V, exceeding the ISO11898 specification of -2V to +7V, and well suited for applications where ground planes from different systems are shifting relative to each other.
This Maxim Integrated CAN family incorporates a fault detection feature for overcurrent, overvoltage and transmission failure, in addition to other options that address key CAN application requirements. This includes low-current standby mode, improved EMI performance, silent mode, remote self diagnostics and more. The family of devices operate over the -40°C to +125°C temperature range.
Visit http://www.FutureElectronics.com/subscribe to receive the latest Future Electronics newsletters and continuously stay up to date with the latest innovations of the technology world. To see the entire portfolio of components available through Future Electronics, visit www.FutureElectronics.com.
About Future Electronics
Future Electronics is a global leader in electronics distribution, recognized for providing customers with global supply chain solutions, custom-tailored engineering services and a comprehensive suite of passives and semiconductor products. Founded by Robert Miller in 1968, Future Electronics has over 5,500 employees and operates in 170 offices in 44 countries around the world. Future Electronics is globally integrated, with a unified IT infrastructure that delivers real-time inventory availability and access to customers. With the highest level of service, the most advanced engineering capabilities, and the largest available-to-sell inventory in the world, Future’s mission is always to Delight the Customer®. For more information, visit www.FutureElectronics.com.
Media Contact
Martin H. Gordon
Director, Corporate Communications
FUTURE ELECTRONICS
www.FutureElectronics.com
514-694-7710 (ext. 2236)
Fax: 514-630-2671
martin.gordon@FutureElectronics.com