Future Electronics Introduces STRADELLA Dense Lens Arrays from LEDiL

Montreal, Canada – May , 2018 – Future Electronics, a global leading distributor of electronic components, is pleased to announce the availability of LEDiL’s STRADELLA family of LEDs.

STRADELLA is a cost-efficient product family of single lenses and dense lens arrays for street, area and industrial lighting. They are an ideal option for up to 3535 size mid and high-power LEDs and CSP LEDs.

Future Electronics customers will benefit from the STRADELLA line’s ability to deliver a huge amount of light from a relatively small area. Bigger lens arrays come with an integrated silicone gasket for dusty and damp environments.

The STRADELLA-IP-28 100 x 100 mm lens module features very high optic density and an integrated silicone gasket for up to IP67 ingress protection. They are fastened with eight M3 size screws and have pockets and channels for connectors and wires.

Typical lumen outputs are over 8000 lm at 700mA for the 3535 high-power LED, and 2800 to 4000 lm for the 3030 mid-power LED. HB variants are also compatible with CSP LEDs.

LEDiL’s STRADELLA LEDs are available now from Future Electronics. For more information and to watch a video about this product, click here. To see the entire portfolio of LEDiL products available through Future Electronics, visit: www.FutureElectronics.com

About Future Electronics

Future Electronics is a global leader in electronics distribution, ranking 3rd in component sales worldwide, with an impressive reputation for developing efficient, comprehensive global supply chain solutions, as well as differentiated engineering services encompassing technical support, technology training and custom board design. Founded in 1968 by Robert Miller, President, Future Electronics has established itself as one of the most innovative organizations in the industry today, with 5,500 employees in 169 offices in 44 countries around the world. Future Electronics is globally integrated, with one worldwide IT infrastructure providing real-time inventory availability and access, while enabling full integration of its operations, sales and marketing worldwide. Offering the highest level of service, the most advanced engineering capabilities and technical solutions through all stages of the design-production cycle, and the largest available-to-sell inventory in the world, Future’s mission is always to Delight the Customer®. For more information, visit www.FutureElectronics.com.

 

Media Contact
Martin H. Gordon
Director, Corporate Communications
FUTURE ELECTRONICS
www.FutureElectronics.com

514-694-7710 (ext. 2236)
Fax: 514-630-2671
martin.gordon@FutureElectronics.com