Montreal, Canada – June 7, 2018 – Future Electronics, a global leading distributor of electronic components, is pleased to offer the latest die-cast aluminum enclosures from Bud Industries.
These aluminum enclosures are resistant to atmospheric and marine corrosion, and are ideal for housing sensitive electronic assemblies and pneumatic, hydraulic, and electrical devices in both commercial and industrial environments. They are IP68 rated, and meet NEMA/UL Type 4x, 6, 6P, 12 and 13 requirements.
Customers of Future Electronics can also modify and customize these enclosures with the assistance of their Future salesperson.
The AN-series features a hinged cover, which allows for easy access without risk of damage to the cover. The included external mounting brackets allow the box to be mounted on a wall or panel without having to remove the cover and expose internal components to the environment. They are available in black powder coat finish, and are easily machined and modified to your particular requirements.
Bud Industries aluminum enclosures are available now from Future Electronics. For more information and to watch a video about this product, click here. To see the entire portfolio of Bud Industries products available through Future Electronics, visit: www.FutureElectronics.com
About Future Electronics
Future Electronics is a global leader in electronics distribution, ranking 3rd in component sales worldwide, with an impressive reputation for developing efficient, comprehensive global supply chain solutions, as well as differentiated engineering services encompassing technical support, technology training and custom board design. Founded in 1968 by Robert Miller, President, Future Electronics has established itself as one of the most innovative organizations in the industry today, with 5,500 employees in 169 offices in 44 countries around the world. Future Electronics is globally integrated, with one worldwide IT infrastructure providing real-time inventory availability and access, while enabling full integration of its operations, sales and marketing worldwide. Offering the highest level of service, the most advanced engineering capabilities and technical solutions through all stages of the design-production cycle, and the largest available-to-sell inventory in the world, Future’s mission is always to Delight the Customer®. For more information, visit www.FutureElectronics.com.
Media Contact
Martin H. Gordon
Director, Corporate Communications
FUTURE ELECTRONICS
www.FutureElectronics.com
514-694-7710 (ext. 2236)
Fax: 514-630-2671
martin.gordon@FutureElectronics.com